Write/Read |
About Citifiles |
Description |
This command is replaced with SaveData Method Specifies the format of subsequent citifile saves using app.SaveCitiFormattedData |
VB Syntax |
pref.CitiFormat = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(string) - Format in which the citifile will be saved with subsequent save commands. Choose from: "MA" - Linear Magnitude / degrees "DB" - Log Mag / degrees "RI" - Real / Imaginary "Auto" - Format in which the trace is already displayed. If other than Log Mag, Linear Magnitude, or Real/Imag, then the format will be in Real/Imag. |
Return Type |
String |
Default |
"Auto" |
Examples |
pref.CitiFormat = "MA" 'Write |
|
format = pref.CitiFormat 'Read |
|
C++ Syntax |
HRESULT get_CitiFormat(BSTR *Format) |
Interface |
IPreferences |