Write/Read
About Fixturing

CmnModeZConvState Property


Description

Turns ON or OFF 4-port common port impedance conversion function. Must also set the fixture simulator function to ON using FixturingState Property.

 VB Syntax

fixture.CmnModeZConvState = value

Variable

(Type) - Description

fixture

A Fixturing (object)

value

(Boolean)

False - Turns common port impedance conversion OFF

True - Turns common port impedance conversion ON

Return Type

Boolean

Default

False

Examples

fixture.CmnModeZConvState = False 'Write

value = fixture.CmnModeZConvState 'Read

C++ Syntax

HRESULT get_CmnModeZConvState( VARIANT_BOOL *pVal)

HRESULT put_CmnModeZConvState( VARIANT_BOOL newVal)

Interface

IFixturing2