Write/Read |
About Ext DC Devices |
Description |
Sets and returns the DC Type for an external DC Device which can be configured as either a DC Meter or a DC Source. This setting is used as the units for display on the PNA X-axis. |
VB Syntax |
extDC.DCType = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(String) DC type. Choose from: "dBm", "A", "V", "W", "K", "F", "C" |
Return Type |
String |
Default |
"V" |
Examples |
extDC.DCType = "A" 'Write |
|
units = extDC.DCType 'Read |
|
C++ Syntax |
HRESULT get_DCType (BSTR *pValue) HRESULT put_DCType (BSTR newVal) |
Interface |
IExternalDCDevice |
Last Modified:
|
15-Feb-2012 |
New topic |