Read only |
About Help, About PNA |
Description |
Returns the DSP Revision number that is visible in the Help, About Network Analyzer dialog box. Learn more. |
VB Syntax |
value = cap.DspRevision |
Variable |
(Type) - Description |
|
value |
(String) - Variable to store the returned DSP revision number. |
|
cap |
A Capabilities (object) |
Return Type |
String |
Default |
Not Applicable |
Examples |
value = cap.DspRevision 'Read |
C++ Syntax |
HRESULT get_DspRevision(BSTR *value); |
Interface |
ICapabilities6 |