Read-only
About SA Application

DataByteSize Property


Description

Returns the byte size of the data to be exported in binary mode.

Note: Returned number can exceed the maximum integer number size. In that case, an error will be raised. For that reason, we provide an access to larger numbers with the same query and LSB or MSB suffixes.

VB Syntax

value = sa.dft.DataByteSize

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Variant) Variable to store the returned value.

Return Type

Variant

Example

value = sa.dft.DataByteSize 'Read

C++ Syntax

HRESULT get_DataByteSize(VARIANT* val);

Interface

ISpectrumAnalyzerDFT