Write/Read |
About SA Application |
Description |
Enables/disables adding marker data to the text file (*.txt) output. |
VB Syntax |
sa.dft.DataExportMarkersEnabled = value |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
value |
(Boolean) Choose from: 0 - OFF - Disable marker data to the file output. 1 - ON - Enable marker data to the file output. |
Return Type |
Boolean |
Default |
OFF |
Examples |
sa.dft.DataExportMarkersEnabled = ON 'Write |
|
value = sa.dft.DataExportMarkersEnabled 'Read |
|
C++ Syntax |
HRESULT get_DataExportMarkersEnabled(VARIANT_BOOL* enable) |
Interface |
ISpectrumAnalyzerDFT2 |