Read-only
About SA Application

DataFirstRFBin Property


Description

Returns the frequency of the first RF bin.

Note: This value can differ slightly from the SA Sweep start frequency, the frequency of the first RF bin is aligned with the current DFT grid.

VB Syntax

value = sa.dft.DataFirstRFBin

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Double) Variable to store the returned value.

Return Type

Double

Example

value = sa.dft.DataFirstRFBin 'Read

C++ Syntax

HRESULT get_DataFirstRFBin(double* val);

Interface

ISpectrumAnalyzerDFT