Read-only |
About FIFO |
Description |
Reads FIFO data the same as Data Property but returns the data in a more compact form of SAFEARRAY. This is significantly faster but it is not supported in all client environments. |
VB Syntax |
array = fifo.DataInCompactForm (count) |
Variable |
(Type) - Description |
|
array |
(Variant) Variable to store the returned data |
|
fifo |
A FIFO Object |
|
count |
(Long Integer) Number of data points to read. |
Return Type |
Returns an array of 4 byte floating point numbers. |
Default |
Not Applicable |
Examples |
value = fifo.DataInCompactForm(500) 'Read |
C++ Syntax |
HRESULT get_DataInCompactForm(long count,VARIANT * data); |
Interface |
IFIFO |