Write/Read |
About PNA-X Pulsed Capabilities |
Description |
Sets the pulse delay - the amount of time before a new pulse begins. |
VB Syntax |
pulse.Delay(n) = value |
Variable |
(Type) - Description |
|
pulse |
A PulseGenerator (object) |
|
n |
(Integer) Pulse generator number. Choose from 0 to 4. Or use PulseGeneratorID to refer to an external pulse generator. 0 is the generator that pulses the ADC. |
|
value |
(Double) Delay value in seconds. Choose a value from about 33ns to about 70 seconds. |
Return Type |
Double |
Default |
0 |
Examples |
pulse.Delay(1) = 1ms 'Write |
|
value = pulse.Delay(4) 'Read |
|
C++ Syntax |
HRESULT get_Delay(integer pulse, double* delay); HRESULT put_Delay(integer pulse, double delay); |
Interface |
IPulseGenerator |