Write/Read |
About Swept IMD |
Description |
Sets and returns the fixed tone spacing value. Use with IMD sweep types:
|
VB Syntax |
object.DeltaFrequency = value |
Variable |
(Type) - Description |
|
object |
A SweptIMD or IMSpectrum Object |
|
value |
(Double) - Tone spacing frequency in Hz. Both the F1 and F2 tones MUST be within the frequency range of the PNA. |
Return Type |
Double |
Default |
1 MHz |
Examples |
imd.DeltaFrequency = 1e6 'Write |
|
value = imd.DeltaFrequency 'Read |
|
C++ Syntax |
HRESULT get_DeltaFrequency(double *pVal) |
Interface |
ISweptIMD IIMSpectrum |