Write-Read

DisplayGlobalPassFail Property


Description

Shows or hides the dialog which displays global pass/fail results. Learn more about Global Pass/Fail.

 VB Syntax

app.DisplayGlobalPassFail = value

Variable

(Type) - Description

app

An Application (object)

value

(Boolean)

True - displays the pass/fail dialog.

False -  hides the pass/fail dialog.

Return Type

Boolean

Default

False

Examples

Dim app As Application

Set app = New Application

app.DisplayGlobalPassFail = true  'shows dialog

C++ Syntax

HRESULT get_DisplayGlobalPassFail(VARIANT_BOOL * Val);

HRESULT put_DisplayGlobalPassFail(VARIANT_BOOL Val);

Interface

IApplication6