Read-only |
About Marker Search |
Description |
Returns the Q (quality factor) result of the SearchBandwidth method. The Q factor is the ratio of Center Frequency to Bandwidth (Center Frequency / Bandwidth). |
VB Syntax |
filtQ = meas.FilterQ |
Variable |
(Type) - Description |
filtQ |
(single) - Variable to store bandwidth Q data |
meas |
A Measurement (object) |
Return Type |
Single |
Default |
Not applicable |
Examples |
filtQ = meas.FilterQ 'Read |
C++ Syntax |
HRESULT get_FilterQ(float* quality) |
Interface |
IMeasurement |