Write/Read |
About Swept IMD |
Description |
Sets and returns the stop frequency when sweeping the main tones. Use with sweep type = naIMDToneCenterFreqSweep. |
VB Syntax |
imd.FrequencyCenterStop = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMD Object |
|
value |
(Double) Stop frequency in Hz. The F1 and F2 tones MUST be within the frequency range of the PNA. |
Return Type |
Double |
Default |
26.4995 MHz |
Examples |
imd.FrequencyCenterStop = 20e9 'Write |
|
value = imd.FrequencyCenterStop 'Read |
|
C++ Syntax |
HRESULT get_FrequencyCenterStop(double *pVal) |
Interface |
ISweptIMD |