Write/Read |
About Swept IMD |
Description |
Sets and returns the frequency span when sweeping the main tones. Use with sweep type = naIMDToneCenterFreqSweep. |
VB Syntax |
imd.FrequencyCenterSpan = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMD Object |
|
value |
(Double) Frequency span in Hz. The F1 and F2 tones MUST be within the frequency range of the PNA. |
Return Type |
Double |
Default |
26.489 GHz |
Examples |
imd.FrequencyCenterSpan = 10e9 'Write |
|
value = imd.FrequencyCenterSpan 'Read |
|
C++ Syntax |
HRESULT get_FrequencyCenterSpan(double *pVal) |
Interface |
ISweptIMD |