Write/Read
About Frequency Offset

FrequencyOffsetDivisor Property  Superseded


Description

This method is replaced by properties on the FOMRange Object.

Specifies (along with FrequencyOffsetMultiplier) the value to multiply by the stimulus.

See other Frequency Offset properties

 VB Syntax

object.FrequencyOffsetDivisor  = value

Variable

(Type) - Description

object

Channel (object)

or

CalSet (object) - Read-only property

value

(Double) - Divisor value. Range is 1 to 1000

Return Type

Double

Default

1

Examples

chan.FrequencyOffsetDivisor = 2 'Write

fOffsetDiv = chan.FrequencyOffsetDivisor 'Read

C++ Syntax

HRESULT get_FrequencyOffsetDivisor(double*pval)

HRESULT put_FrequencyOffsetDivisor(double newVal)

Interface

IChannel2

|CalSet3