Write/Read
About Frequency Offset

FrequencyOffsetMultiplier Property  Superseded


Description

This method is replaced by properties on the FOMRange Object.

Specifies (along with FrequencyOffsetDivisor) the value to multiply by the stimulus. See other Frequency Offset properties.

 VB Syntax

object.FrequencyOffsetMultiplier  = value

Variable

(Type) - Description

object

Channel (object)

or

CalSet (object) - Read-only property

value

(Double) - Multiplier value. Range is 1 to 1000

Return Type

Double

Default

1

Examples

chan.FrequencyOffsetMultiplier = 2 'Write

fOffsetMult = chan.FrequencyOffsetMultiplier 'Read

C++ Syntax

HRESULT get_FrequencyOffsetMultiplier (double*pval);
HRESULT put_FrequencyOffsetMultiplier (double newVal);

Interface

IChannel2

|CalSet3