Write/Read

 

FrequencyOffsetRangeForCalComputations Property


Description

Specifies the FOM frequency range to use when performing calibration.

 VB Syntax

pref.FrequencyOffsetRangeForCalComputations = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Enum as NACalFOMRange) - Choose from:

0 - naCalFOMRangeAuto - All other calibration situations.

1 - naCalFOMRangePrimary - Used for calibrating at the mmWave frequencies when NOT using a test set. Learn more.

Return Type

Enum

Default

naCalFOMRangeAuto

Examples

pref.FrequencyOffsetRangeForCalComputations = naCalFOMRangePrimary 'Write

calPref = pref.FrequencyOffsetRangeForCalComputations 'Read

C++ Syntax

HRESULT get_FrequencyOffsetRangeForCalComputations(tagNACalFOMRange * val);

HRESULT put_FrequencyOffsetRangeForCalComputations((tagNACalFOMRange val);

Interface

IPreferences10