Read-only
About Marker Search

GainMax Property


Description

Returns the GainMax result of the PNOP or PSAT marker search.

Gain Max =  PMax Out - PMax In

 VB Syntax

gainMax = pMarker.GainMax

Variable

(Type) - Description

gainMax

(double) - Variable to store returned value

pMarker

A PNOP (object) or PSaturation (Object)

Return Type

Double

Default

Not applicable

Examples

gainMax = pMarker.GainMax 'Read

See example program

C++ Syntax

HRESULT get_GainMax(double* pNewVal)

Interface

IPNOP or IPSaturation