Read-only
About Swept IMD

HighestOrderProduct Property


Description

Returns the highest order product that can be measured by SweptIMD.

 VB Syntax

value = imd.HighestOrderProduct

Variable

(Type) - Description

value

(Long Integer) Variable in which to store the returned value.

imd

A SweptIMD Object

Return Type

Integer

Default

Always returns 9

Examples

value = imd.HighestOrderProduct 'Read

C++ Syntax

HRESULT get_HighestOrderProduct(long *pVal)

Interface

ISweptIMD