Write/Read |
About IF Bandwidth |
Description |
Sets or returns the IF Bandwidth of the channel. Sets or returns the IF Bandwidth of the segment. Returns the IF Bandwidth used in the Cal Set |
VB Syntax |
object.IFBandwidth = value |
Variable |
(Type) - Description |
|
object |
Channel (object) or Segment (object) or CalSet (object) - Read-only property |
|
value |
(double) - IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the PNA model. (Click to see the lists.) If an invalid number is specified, the analyzer will round up to the closest valid number. |
Return Type |
Double |
Default |
Varies with PNA model. |
Examples |
chan.IFBandwidth = 3e3 'sets the IF Bandwidth of for the channel object to 3 kHz. -Write |
|
ifbw = chan.IFBandwidth -Read |
|
C++ Syntax |
HRESULT get_IFBandwidth(double *pVal); HRESULT put_IFBandwidth(double newVal); |
Interface |
IChannel |CalSet3 |