Read only |
About PNA Options |
Description |
Returns the number of internal DC receivers in the analyzer. |
VB Syntax |
value = cap.InternalDCReceiverCount |
Variable |
(Type) - Description |
|
value |
(Long) - Variable to store the returned value. |
|
cap |
A Capabilities (object) |
Return Type |
Long |
Default |
Not Applicable |
Examples |
value = cap.InternalDCReceiverCount 'Read |
C++ Syntax |
HRESULT get_InternalDCReceiverCount(long *value); |
Interface |
ICapabilities14 |