Read-only |
About Trigger |
Description |
Returns whether or not a channel is in hold mode. To set the channel to hold mode, use Hold Method. |
VB Syntax |
value = chan.IsHold |
Variable |
(Type) - Description |
|
value |
(boolean) - Choose either: False - Channel trigger is NOT set to hold. True - Channel trigger IS set to hold. |
|
chan |
Channel (object) |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
trig = chan.IsHold 'Read |
C++ Syntax |
HRESULT get_IsHold ( VARIANT_BOOL *bHold); |
Interface |
IChannel4 |
Last Modified:
|
11-Nov-2014 |
Edited IChannel 3 to 4 |