Read only |
About PNA Options |
Description |
Returns a value indicating the presence of Receiver step attenuators in the remote PNA. |
VB Syntax |
value = cap.IsReceiverStepAttenuatorPresent (n) |
Variable |
(Type) - Description |
|
value |
(Boolean) - Variable to store the returned value. True - Receiver step attenuators are present. False - Receiver step attenuators are not present. |
|
cap |
A Capabilities (object) |
|
n |
(Long) - port number to query for step attenuators |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
value = cap.IsReceiverStepAttenuatorPresent(1)'Read |
C++ Syntax |
HRESULT get_IsReceiverStepAttenuatorPresent(long portNumber, VARIANT_BOOL * present ); |
Interface |
ICapabilities |