Read only |
About PNA Options |
Description |
Returns a value indicating the presence of a Reference Bypass Switch in the remote PNA. |
VB Syntax |
value = cap.IsReferenceBypassSwitchPresent (n) |
Variable |
(Type) - Description |
|
value |
(Boolean) - Variable to store the returned value. True - Reference Bypass Switch is present. False - Reference Bypass Switch is not present. |
|
cap n |
A Capabilities (object) (Long) - port number to query for reference bypass switch |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
value = cap.IsReferenceBypassSwitchPresent(1) 'Read |
C++ Syntax |
HRESULT get_IsReferenceBypassSwitchPresent(long portNumber, VARIANT_BOOL * present ); |
Interface |
ICapabilities |