Read-only |
Description |
Designed to be used for an iterative cal standard such as a sliding load, this command returns the number of iterative measurement acquisitions that has been made for the specified step. Zero (0) is returned if the step has not yet been measured. For most cal steps that have already been measured, this command returns 1. To count acquisition steps, set SlidingLoadAcquisitionBehavior. |
VB Syntax |
value = guided.IterationCountForStep (n) |
Variable |
(Type) - Description |
|
value |
(Long) Variable to store the returned number of iterations that have been measured for the step. |
|
guided |
GuidedCalibration (object) |
|
n |
Guided Cal step number for which the acquisition number will be returned. Use GenerateSteps Method to read the number of steps in the calibration. |
Return Type |
Long |
Default |
Not Applicable |
Examples |
value = obj.IterationCountForStep(4) |
C++ Syntax |
HRESULT get_IterationCountForStep (long step, long *iterations); |
Interface |
IGuidedCalibration10 |
Last Modified:
|
4-Dec-2012 |
New topic |