Read-only |
About LXI |
Description |
Returns information about the current status of the PNA’s computer networking configuration. This is the same set of information that is returned in an NA_IPConfiguration data structure by the GetIPConfigurationStruct method. |
VB Syntax |
value = app.LANConfiguration |
Variable |
(Type) - Description |
|
value |
(String) Variable to contain the PNA’s LAN configuration string |
|
app |
An Application (object) |
Return Type |
Comma-delimited string |
Default |
Not Applicable |
Examples |
networkConfigInfo = app.LANConfiguration |
C++ Syntax |
HRESULT get_LANConfiguration (BSTR * pStrConfig); |
Interface |
IApplication13 |