Read-only
About Embedded LO

LODeltaFound Property


Description

Returns the LO frequency delta from the specified tuning sweep.

 VB Syntax

value = embedLODiag.LODeltaFound (n)

Variable

(Type) - Description

value

(Double) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

n

(Long) Tuning sweep number. Use NumberOfSweeps to find the number of sweeps taken.

Default

Not Applicable

Examples

data= embedLO.LODeltaFound 3 'read

C++ Syntax

HRESULT LODeltaFound(long sweep, double* deltaLO);

Interface

IEmbededLODiagnostic