Write/Read
About Mixer Configuration

LOPower Property


Description

Sets or returns the value of LO Power.

 VB Syntax

obj.LOPower (n) = value

Variable

(Type) - Description

obj

A Mixer Interface pointer to the Measurement (object)

Or

A Converter Object

n

(Long)  - LO stage number

Choose from 1 or 2

value

(double) - LO Power in dBm.

Return Type

Double

Default

-10dBm

Examples

Print mixer.LOPower(1) 'prints the value of the LO Power

C++ Syntax

HRESULT get_LOPower(double *pVal)

HRESULT put_LOPower(double newVal)

Interface

IMixer

IConverter