Write/Read |
About LXI |
Description |
Opens and closes the LAN Status dialog with the LAN Status Indicator showing IDENTIFY. The PNA supports this capability to satisfy a requirement of the LAN eXtensions for Instrumentation (LXI) standard. Changing the value of this property is the same operation that occurs when clicking the Toggle LXI Identification button on the Welcome web page presented by the PNA web server. |
VB Syntax |
app.LXIDeviceIDState = bool |
Variable |
(Type) - Description |
|
app |
An Application (object) |
bool |
(boolean) Choose from: True - Displays the LAN Status dialog with the Status Indicator showing IDENTIFY. False -
|
Return Type |
Boolean |
Default |
False |
Examples |
app.LXIDeviceIDState = True 'Write value = app.LXIDeviceIDState 'Read |
C++ Syntax |
HRESULT get_LXIDeviceIDState( VARIANT_BOOL* pState); HRESULT put_LXIDeviceIDState( VARIANT_BOOL state); |
Interface |
IApplication14 |