Write/Read
About DC Sources

LimitMin Property


Description

Sets and returns the Min DC limit value for a DC source.

 VB Syntax

dc.LimitMin(deviceName) = value

Variable

(Type) - Description

dc

A DCStimulus (object)

deviceName

(String) Name of the "DC source"

Use Source Property to read a list of configured DC source names.

value

(Double) Min DC limit value. Choose a value within the range of the DC source.

Return Type

Double

Default

-10

Examples

dc.LimitMin("myDCSource") = -10 'Write

value = dc.LimitMin("myDCSource") 'Read

C++ Syntax

HRESULT get_LimitMin(BSTR deviceName, double* value);

HRESULT put_LimitMin(BSTR deviceName, double value);

Interface

IDCStimulus2