Write/Read |
About Integrated Pulsed App |
Description |
Sets the pulse repetition frequency (PRF) for ALL internal pulse generators. This setting is equal to 1/period which is set with MasterPeriod Property Note: On the Pulse Setup dialog, this command is a "Basic" setting, intended to be used with the 'Auto' selections set to ON. |
VB Syntax |
pulse.MasterFrequency = value |
Variable |
(Type) - Description |
|
pulse |
A PulseMeasurementControl (object) |
|
value |
(Double) PRF in Hz. |
Return Type |
Double |
Default |
1 kHz |
Examples |
pulse.MasterFrequency = 1e4 'Write |
|
value = pulse.MasterFrequency 'Read |
|
C++ Syntax |
HRESULT get_MasterFrequency(double* value); HRESULT put_MasterFrequency(double value); |
Interface |
IPulseMeasurementControl2 |
Last modified:
|
11-May-2011 |
New topic |