Write/Read |
About Integrated Pulsed App |
Description |
Sets the pulse width for ALL internal pulse generators. Note: On the Pulse Setup dialog, this command is a 'Basic setting, which is intended to be used with the 'Auto' selections set to ON. |
VB Syntax |
pulse.MasterWidth = value |
Variable |
(Type) - Description |
|
pulse |
A PulseMeasurementControl Object (object) |
|
value |
(Double) Pulse width in seconds. |
Return Type |
Double |
Default |
100 microseconds |
Examples |
pulse.MasterWidth = 1e-3 'Write |
|
value = pulse.MasterWidth 'Read |
|
C++ Syntax |
HRESULT get_MasterWidth(double* MasterWidth); HRESULT put_MasterWidth(double MasterWidth); |
Interface |
IPulseMeasurementControl2 |
Last modified:
|
9-May-2011 |
New topic |