Write/Read
About External DC Devices

MaxOutputState Property


Description

Sets and returns the "Define Max As" ON/OFF state for an external DC Source.

 VB Syntax

extDC.MaxOutputState = value

Variable

(Type) - Description

extDC

An ExternalDCDevice (object)

value

(Boolean) "Define Max As" ON/OFF state. Choose from:

True - Turn "Define Max As" ON

False - Turn "Define Max As" OFF

Return Type

Boolean

Default

True

Examples

extDC.MaxOutputState = True 'Write

value = extDC.MaxOutputState 'Read

C++ Syntax

HRESULT get_MaxOutputState(VARIANT_BOOL *value)

HRESULT put_MaxOutputState(VARIANT_BOOL value)

Interface

IExternalDCDevice3