Write/Read
About External DC Devices

MaxOutput Property


Description

Sets and returns the "Define Max As" value for an external DC Source.

 VB Syntax

extDC.MaxOutput = value

Variable

(Type) - Description

extDC

A ExternalDCDevice (object)

value

(Double) Maximum value for the external DC Source.

Return Type

Double

Default

10 V

Examples

extDC.MaxOutput = 10 'Write

value = extDC.MaxOutput 'Read

C++ Syntax

HRESULT get_MaxOutput( double* value);

HRESULT put_MaxOutput( double value);

Interface

IExternalDCDevice3