Read/Write
About Embedded LO

MaxPreciseTuningIterations Property


Description

Sets and returns the maximum number of tuning iterations to achieve the precise tolerance.

 VB Syntax

obj.MaxPreciseTuningIterations = value

Variable

(Type) - Description

obj

An EmbeddedLO (object) or

A ConverterEmbeddedLO (object)

value

(Long) Maximum number of tuning iterations.

Return Type

(Long)

Default

5

Examples

embedLO.MaxPreciseTuningIterations = 3 'write

value = embedLO.MaxPreciseTuningIterations 'read

C++ Syntax

HRESULT get_MaxPreciseTuningIterations long* iter);

HRESULT put_MaxPreciseTuningIterations long iter);

Interface

IEmbededLO