Write/Read |
About Source Power CalAbout PMAR |
Description |
Set and returns the maximum usable frequency specified for the power sensor. |
VB Syntax |
pwrSensor.MaximumFrequency = value |
Variable |
(Type) - Description |
|
pwrSensor |
A PowerSensor (Object) or a PowerSensorAsReceiver (Object) |
|
value |
(double) -Frequency in Hertz. |
Return Type |
Double |
Default |
Device dependent |
Examples |
pwrSensor.MaximumFrequency = 6e9 'Write MaxFreq = pwrSensor.MaximumFrequency 'Read |
C++ Syntax |
HRESULT put_MaximumFrequency(double newVal); HRESULT get_MaximumFrequency(double *pVal); |
Interface |
IPowerSensor IPowerSensorPMAR |