Each power sensor connected to the power meter associated with Source Power Calibration will have a PowerSensor object created to represent it. These PowerSensor objects reside in the PowerSensors collection within the SourcePowerCalibrator object. You cannot directly create PowerSensor objects, but can only retrieve existing ones from the PowerSensors collection.
The PowerSensorCalFactorSegment object is also accessed through the PowerSensor object. These are accessed through the CalFactorSegments collection in the PowerSensor object.
Dim pna As AgilentPNA835x.Application
Set pna = CreateObject("AgilentPNA835x.Application", <analyzerName>)
Dim powerCalibrator as SourcePowerCalibrator
Dim powerSensor as PowerSensor
Dim calFactorSegment as PowerSensorCalFactorSegment
Set powerCalibrator = pna.SourcePowerCalibrator
' Specify GPIB address of the power meter.
powerCalibrator.PowerMeterGPIBAddress = 13
' Each time the PowerSensors collection is accessed, the power meter is queried to determine which channels have sensors attached. The collection is updated accordingly.
If powerCalibrator.PowerSensors.Count > 0 Then
' If channel B of the meter has a sensor attached but channel A does not, then element 1 of the
' collection is sensor B. Whenever channel A has a sensor, sensor A will be element 1.
Set powerSensor = powerCalibrator.PowerSensors(1)
' Insert one new PowerSensorCalFactorSegment at the beginning of the collection (index 1).
powerSensor.CalFactorSegments.Add(1)
' Assign our variable to refer to that object.
Set calFactorSegment = powerSensor.CalFactorSegments(1)
' Set property values for that object.
calFactorSegment.Frequency = 300000
' frequency in Hz
calFactorSegment.CalFactor = 98
' cal factor in percent
End If
(Bold Methods or Properties provide access to a child object)
Methods |
Interface |
Description |
|---|---|---|
|
None |
|
|
Properties |
Interface |
Description |
|
IPowerSensor |
Collection for iterating through the segments of a power sensor cal factor table. |
|
|
IPowerSensor |
Maximum usable frequency (Hz) specified for this power sensor. |
|
|
IPowerSensor |
Minimum usable frequency (Hz) specified for this power sensor. |
|
|
IPowerSensor |
Identifies which power sensor this object corresponds to ( or which channel of the power meter the sensor is connected to). |
|
|
IPowerSensor |
Reference cal factor (%) associated with this power sensor. |
|
Interface |
Introduced with PNA Rev: |
|
IPowerSensor |
2.0 |