Read only |
About PNA Options |
Description |
Returns the maximum amount of receiver attenuation. |
VB Syntax |
value = cap.MaximumReceiverStepAttenuator (n) |
Variable |
(Type) - Description |
|
value |
(Double) - Variable to store the returned value of maximum receiver attenuation. |
|
cap |
A Capabilities (object) |
|
n |
(Long) - port number to query for step attenuators |
Return Type |
Double |
Default |
Not Applicable |
Examples |
value = cap.MaximumReceiverStepAttenuator'Read |
C++ Syntax |
HRESULT get_MaximumReceiverStepAttenuator(long portNumber, double * attenuation ); |
Interface |
ICapabilities |