Write/Read
About SA Application

MemShareName Property


Description

Assigns a specified name to the Microsoft Windows shared data mechanism when MemShareEnabled is enabled.

VB Syntax

sa.dft.MemShareName = MemFileName

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

MemFileName

(String) Memory file name.

Return Type

String

Example

sa.dft.MemShareName = "Mem_Share" 'Write

name = sa.dft.MemShareName 'Read

C++ Syntax

HRESULT get_MemShareName(BSTR* MemFileName);

HRESULT put_MemShareName(BSTR MemFileName);

Interface

ISpectrumAnalyzerDFT