Write/Read
About External DC Devices

MinOutputState Property


Description

Sets and returns the "Define Min As" ON/OFF state for an external DC Source.

 VB Syntax

extDC.MinOutputState = value

Variable

(Type) - Description

extDC

An ExternalDCDevice (object)

value

(Boolean) "Define Min As" ON/OFF state. Choose from:

True - Turn "Define Min As" ON

False - Turn "Define Min As" OFF

Return Type

Boolean

Default

True

Examples

extDC.MinOutputState = True 'Write

value = extDC.MinOutputState 'Read

C++ Syntax

HRESULT get_MinOutputState(VARIANT_BOOL *value)

HRESULT put_MinOutputState(VARIANT_BOOL value)

Interface

IExternalDCDevice3