Write/Read |
About Source Power CalAbout PMAR |
Description |
Sets and returns the minimum usable frequency specified for the power sensor. |
VB Syntax |
pwrSensor.MinimumFrequency = value |
Variable |
(Type) - Description |
|
pwrSensor |
A PowerSensor (Object) or A PowerSensorAsReceiver (Object) |
|
value |
(double) -Frequency in Hertz. |
Return Type |
Double |
Default |
Device dependent |
Examples |
pwrSensor.MinimumFrequency = 300e3 'Write MinFreq = pwrSensor).MinimumFrequency 'Read |
C++ Syntax |
HRESULT put_MinimumFrequency(double newVal); HRESULT get_MinimumFrequency(double *pVal); |
Interface |
IPowerSensor IPowerSensorPMAR |