Read-only
About Pulsed Application

MinimumIFFrequency Property


Description

Returns the minimum allowed value for the IFFrequency Property

 VB Syntax

value = IfConfig.MinimumIFFrequency

Variable

(Type) - Description

value

(double) Variable to store the returned minimum allowed frequency that can be applied to the IFFrequency Property.

IfConfig

IFConfiguration (object)

Return Type

Double

Default

Not Applicable

Examples

val = App.ActiveChannel.IFConfiguration.MinimumIFFrequency 'Read

C++ Syntax

HRESULT get_MinimumIFFrequency( double * pMinFreq);

Interface

IIFConfiguration3