Read-only |
Description |
Designed to be used for an iterative cal standard such as a sliding load, this command returns the minimum number of required iterative measurement acquisitions for the specified step. For most connection steps this will return 1, but for an iterative cal standard such as a sliding load, it will return a number such as 5. To count acquisition steps, set SlidingLoadAcquisitionBehavior. |
VB Syntax |
value = guided.MinimumIterationsForStep (n) |
Variable |
(Type) - Description |
|
value |
(Long) Variable to store the returned number of minimum iterations for the step. |
|
guided |
GuidedCalibration (object) |
|
n |
Guided Cal step number for which to return the number of iterative measurement acquisitions that have been made. Use GenerateSteps Method to read the number of steps in the calibration. |
Return Type |
Long |
Default |
Not Applicable |
Examples |
value = obj.MinimumIterationsForStep(4) |
C++ Syntax |
HRESULT get_MinimumIterationsForStep (long step, long *iterations); |
Interface |
IGuidedCalibration10 |
Last Modified:
|
4-Dec-2012 |
New topic |