Write-only |
About SMC Phase |
Description |
Set the filename of the S2P file used to characterize the calibration mixer |
VB Syntax |
smc.MixerCharacterizationFile = value |
Variable |
(Type) - Description |
|
smc |
An SMCType (object) |
|
value |
(String) Full path, file name, and extension of the mixer characterization file. |
Return Type |
String |
Default |
Not applicable |
Example |
SMC.MixerCharacterizationFile = "C:/Program Files/Keysight/Network Analyzer/Documents/default.S2P" |
C++ Syntax |
HRESULT put_MixerCharacterizationFile(BSTR Value); |
Interface |
SMCType5 |
Last Modified:
|
25-Mar-2010 |
MX New topic |