Contains the methods and properties to perform an Scalar Measurement Calibration for the Frequency Converter Application (option 083).
See an example which creates and calibrates an SMC measurement.
You can also do the following:
Set app = CreateObject("AgilentPNA835x.Application") Set CalMgr = app.GetCalManager Set guidedCal = CalMgr.CreateCustomCalEx(1) Set SMC = guidedCal.CustomCalConfiguration SMC.ConnectorType(1) = "APC 3.5 male" |
Methods |
Interface |
Description |
---|---|---|
ISMCType |
Acquire the measurement data for the specified step in the calibration process. |
|
ISMCType |
Generates the error terms for the calibration. |
|
ISMCType |
Returns the number of steps required to complete the calibration. |
|
ISMCType |
Returns the description of the specified step calibration process. |
|
ISMCType4 |
Imports separate power meter data for SMC cal. |
|
ISMCType |
Begins a calibration. |
|
Properties |
|
Description |
ISMCType |
Sets ECAL module automatic orientation ON or OFF. |
|
ISMCType |
Sets or returns the calibration source port for the calibration. |
|
ISMCType |
Sets and returns a calibration kit type for calibration. |
|
ISMCType |
Returns a list of cal kits that are compatible with the connector type for the specified port. |
|
ISMCType |
Sets or queries the connector type for the specified port. |
|
ISMCType |
Superseded - Replaced by CalKitType Specify ECAL or Mechanical calibration. |
|
ISMCType |
Superseded - Replaced by CalKitType Specifies the characterization data within an ECal module to be used for the calibration. |
|
ISMCType |
Specifies which port of the ECal module is connected to which port of the PNA when the AutoOrient property = False. |
|
ISMCType5 |
Enable LO Power Cal |
|
ISMCType5 |
Set and return the known delay through the calibration mixer. |
|
ISMCType5 |
Set the filename of the S2P file used to characterize the calibration mixer. |
|
ISMCType2 |
Specifies the S2P filename to embed or de-embed on the input or output of your mixer measurement. |
|
ISMCType2 |
Embed (add) or de-embed (remove) circuit network effects on the input and output of your mixer measurement. |
|
ISMCType |
Superseded - Replaced by SetIsolationPaths and GetIsolationPaths Sets and returns whether Isolation portion of the calibration will be performed or not. |
|
ISMCType4 |
Use a Thru standard or to use two power sensor connections during the SMC power cal |
|
ISMCType |
Superseded - Replaced by PathThruMethod Property Sets and returns the method for performing the thru portion of the calibration. |
|
ISMCType |
Returns a list of connector types for which there are calibration kits. |
Interface |
Introduced with PNA Rev: |
ISMCType |
3.5 |
ISMCType2 |
6.0 |
ISMCType4 |
9.0 |