Write/Read
About SA Application

MultiToneEnable Property


Description

Enables/disables multitone image rejection. When enabled, the window type is set to No Window and the list of RBW possible values is recomputed according to the multitone spacing. When disabled, the window type is set back to what it was before enabling and the RBW list is also set to the previous setting.

 VB Syntax

sa.coherence.MultiToneEnable = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Boolean) Choose from:

0 - OFF - Multitone image rejection disabled.

1 - ON - Multitone image rejection enabled.

Return Type

Boolean

Default

OFF

Examples

sa.coherence.MultiToneEnable = ON 'Write

value = sa.coherence.MultiToneEnable 'Read

C++ Syntax

HRESULT get_MultiToneEnable(VARIANT_BOOL* enable)
HRESULT put_MultiToneEnable(VARIANT_BOOL enable)

Interface

ICoherenceSA