Write/Read
About SA Application

MultiToneSpacing Property


Description

Sets and returns the tone spacing of the multitone signal (in Hz). This value is 1/MultiToneImageRejectPeriod.

VB Syntax

sa.coherence.MultiToneSpacing = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Double)  Frequency spacing of multitone signal (in Hz)

Return Type

Double

Default

1000000

Examples

sa.coherence.MultiToneSpacing = 1E6  'Write

value = sa.coherence.MultiToneSpacing 'Read

C++ Syntax

HRESULT put_MultiToneSpacing(double freqval);

HRESULT get_MultiToneSpacing(double* freqval);

Interface

ICoherenceSA