Write/Read
About SA Application

MultiToneNyquistProtection Property


Description

Sets and returns the Nyquist protection level. Avoids Nyquist images of the IF higher order signal to fall back on multitone frequencies. This setting can only be set > 1 if the tone spacing of the multitone is not an integer divider of 100 MHz.

VB Syntax

sa.coherence.MultiToneNyquistProtection = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Long)  Nyquist protection level.

Return Type

Long

Default

0

Examples

sa.coherence.MultiToneNyquistProtection = 2  'Write

value = sa.coherence.MultiToneNyquistProtection 'Read

C++ Syntax

HRESULT put_MultiToneNyquistProtection(long value);

HRESULT get_MultiToneNyquistProtection(long* value);

Interface

ICoherenceSA2