Read-only | 
		About SA Application | 
	
Description | 
		Read the current multitone settings and determine if they are valid or not.  | 
	
VB Syntax | 
		value = sa.coherence.MultitoneSettingsValid  | 
	
Variable | 
		(Type) - Description | 
	
sa.coherence  | 
		A SpectrumAnalyzerCoherence (object)  | 
	
value  | 
		(Long) Variable to store the returned value. A "1" is valid and a "0" is invalid.  | 
	
Return Type | 
		Boolean  | 
	
Example  | 
		value = sa.coherence.MultitoneSettingsValid 'Read  | 
	
C++ Syntax | 
		HRESULT get_MultitoneSettingsValid(VARIANT_BOOL* value);  | 
	
Interface | 
		ICoherenceSA2  |