Read-only
About Path Configurator

Name (PathConfig) Property


Description

Returns the name of the current configuration only if NO individual element settings had been changed since selecting or storing a configuration. When element settings change, the path configuration name is cleared.

 VB Syntax

name = pathConfig.Name

Variable

(Type) - Description

name

(String) Variable to store the returned configuration name.

pathConfig

A PathConfiguration (object)

Return Type

String

Default

'default' - name of the default factory configuration

Examples

name=pathConf.Name

C++ Syntax

HRESULT get_Name(BSTR* ppName)

Interface

IPathConfiguration